I design a BRUShless DRV10964 motor with a speed of 16000RPM, which cannot be started normally. The motor starts intermittently. The coil resistance and inductance of the motor meet the requirements of DRV10964 specification
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I design a BRUShless DRV10964 motor with a speed of 16000RPM, which cannot be started normally. The motor starts intermittently. The coil resistance and inductance of the motor meet the requirements of DRV10964 specification
Hi,
The maximum electrical frequency that DRV10964 can support is 1300 Hz. Can you provide the number of pole pairs of the motor?
Regards,
Vishnu.