in data sheet : over temperature fault section :
If the RETRY bit is set after the temperature has fallen below the OTS threshold, the part re-enables itself after a
fixed delay of 5 s.
my question is : should i enable the driver manually (set enable pin) once the temperature has fallen below the OTS threshold(check fault pin and OTS bit) or it will be not good for driver ?