Other Parts Discussed in Thread: DRV2603
Hi,
I like DRV2624 and I am thinking of using it instead of previously chosen DRV2603.
However I do not need I2C connection and want to run the driver using pwm only.
I see that I2C connection is required to set ERM/LRA mode.
Is there a possibility to set either ERM/LRA without I2C or should I use a driver such as 2603 instead?
Additionally can I use DRV2624 or DRV2603 with ERM in series? Will the device still work in closed loop mode?
Thank you in advance