Hello team,
Customer use DRV8830 but it doesn't move to sleep state when IN1 and IN2 are Low.
Could you estimate a reason?
The situation are;
- IN1 and IN2 are low state
- Vcc=6V, I2C is 3.3V with pullup resister
- Motor operation by I2C is fine
- When applying 3.3V at I2C, the standby current is around 500uA which is out of the spec.
However, when applying 6V or GND, the standby current is around 0.3uA which is within the spec.
The voltage and pull up resister is connected like below picture.
Best regards,
Koyo