Hi Team,
I am confused about the "8.2.2.2 Mortor current trip point" of the DRV8830 datasheet.
Firstly is the IILIMIT and ILIMIT the same? I think IILIMIT is just a typo.
Secondly "To set IILIMIT to 0.5 A" but why does it use 0.9A at "RISENSE = 0.2 V / 0.9 A = 0.22 Ω."?
I think the currenct shoule be all 0.5A or 0.9A.
But according to the description of "To prevent false trips, ILIMIT must be higher than regular operating current."
Does it means that 0.5A is the regular operating current and to prevent false trips, ILIMIT must be higher than 0.5A so it is 0.9A?
Beat Regards,
Tom Liu