Other Parts Discussed in Thread: DRV10987
Hi,
I am attempting to spin a motor that has a maximum rating of 37k RPM. Using the GUI for the EVM, I am unable to get anywhere close to this speed.
The motor has 4 poles (2 pairs), a phase to phase resistance of .306 ohms and a voltage constant of .488 V/kRPM.
Since the DRV10987 has a maximum electrical frequency of 1000 Hz, calculations suggest that the maximum speed this motor can attain is (1000/2) * 60 = 30,000 RPM. I haven't measured the FG out using an o'scope but I estimate the RPM to be around 1500 or so, quite removed from the expected speed.
Am I limited by the motor's parameters in some way or is there something I should be doing differently, such as using an external PWM signal?
Thanks for your assistance,
Adnan