Other Parts Discussed in Thread: DRV10983,
Hi Team,
I can see the Vin spec which is like VCC during load dump (VCC slew rate < 1 V/µs) –0.3 45V on the datasheet.
In this case, is it meets the ISO16750(http://www.compel.ru/wordpress/wp-content/uploads/2017/05/ISO-16750-22010E-.pdf)?
If customer's the battery meets ISO16750, DRV10983 can also meet the load dump criteria. Is it correct?
Thanks,
Uchihara