Other Parts Discussed in Thread: TIDA-00289, DRV8873
Hi team,
My customer is using a solenoid in their application to provide vibration feedback.
I'm considering promoting DRV110 and TIDA-00289 to them. Do we have any automotive rating product of DRV110?
Or can I recommend other DRV product like DRV8873 and refer to SLVAE59 for their application?
The Vsupply is from 12V battery, I peak is 9A
Thanks,
Scarlett