This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8308: Auto disable BLDC driver using FAULTn flag

Part Number: DRV8308


BLDC Motor voltage is 12.5V. Current is 1.5Arms typ. Transient current 4A

We're looking for closed loop SPEED control in motor driver without using external controller.

Questions:

1) Can I short FAULTn  and ENABLE pins together (with pull-up resistor of 4.7K connected to 3.3V rail)? Requirement: Motor should disable when FAULTn flags is asserted by DRV8308

2) Can you share IBIS model for DRV8308?