The TI E2E™ design support forums will undergo maintenance from July 11 to July 13. If you need design support during this time, open a new support request with our customer support center.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV2665: Programmable voltage source with Buck topology

Part Number: DRV2665

Hi,

Could anyone here help me in selecting the correct programmable voltage source for my design with below requirements?

Input signal: I2C

Input voltage: 36 V

Load:

Voltage: 15 V[min] and 30 V[max] 

Current: 1.8 A @ 24 V

Thanks in advance