Hi Team,
Our customer is using DRV8848 in their system to drive two DC motors, during the direction change, we will see some voltage spike on the rising and falling edge on the output pins as below. Our question is as our understanding, there should be internal MOSFET body diode to clamp these spikes, why we still see the spike which can go up to ~15V with VM=12V? Is there any risk for these spikes on the output pins?
Thanks.