Part Number: DRV8323R
Hi,
I am designing with DRV8323RS.
It is not 100% clear from the data sheet, so I want to make sure.
1) internal regulator
What is the purpose of the internal regulator and DVDD on pin 36?
Is it there because it needs an external Cap?
Is it intended to use as the power supply for the internal amplifier? should be connected as input to VREF at pin 26?
2) Ground scheme
PGND should be used for all things power drive? Gate drivers ...
AGND should be used for current sensing?
BGND should be used as GND for the BUCK converter?
DGND? What is connected to DGND?
Thanks!