Other Parts Discussed in Thread: MSP430F5529, , DRV8323
Tool/software: Code Composer Studio
Hi,
I would like to control a brushless motor (36V max / 45A max / 1620W max) with a BOOSTXL-DRV8323RS driver. My question is about the controlleur adpated to this motor driver. Is the MSP430F5529 microcontroller only adapted to this driver as described on the technical document ? I have a CC1352P2 launchpad that I would like to connect it to the BOOSTXL-DRV8323RS. Is it possible ? If not, have you a reference for a motor driver adapted to my launchpad and my motor needs?
The full project is to creat a motorised longboard with a max speed of 30km/h.
Thanks in advance for your answer.
Sincerely,
PERRIN Paul-Emile