Other Parts Discussed in Thread: DRV10983-Q1
Hi,
I am using 15 DRV10983EMVs for several month.
Some of them started to show a strange behavior. When changing the input signal (either analog or via the GUI) the "Speed command" value in the GUI and the "Speed command Buffer" are not the same "even closed loop accelerate" is in Infinite.
The speed command buffer value is staying for minutes at the same level, when I lower the input signal. input increases are accepted faster but als not infinite.