This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8428E: change of KV with different VREF

Part Number: DRV8428E

Good morning,

Today,  I will use the DRV8428E with a  0.330 A curent in the  stepper motor.

            I chopping current = VREF / KV

          with KV  :  transimpedance gain  and        VREF = DVDD * Rref2/( Rref2 + Rref1)

DVDD=5V   Rref2 = 4.99 K    Rref1= 20 K  --> VREF= 5 *4.99(4.99+20) = 0.998V

 the result is :       I chopping current = 0.998/3=  0.333 A

The problem is that   KV ( transimpedance gain)  is defined  only for VREF = 3V      ( data sheet page 8 SLOSE51A – JUNE 2020 – REVISED NOVEMBER 2020)   KV= 3V/A  +- 0.195

Could you please tell me if the value of KV is the same with different  value of   VREF

Thanks in advance for your answer

Michel Thiébaut