Other Parts Discussed in Thread: DRV10970
Hello,
I am attempting to drive a blower motor (datasheet attached) using the DRV10970 evaluation board. From the blower datasheet, I have wired and configured the board to run in 30-deg sinusoidal mode with needing to invert the +/- hall signals. The motor will spin when powered, however, it only spins at one speed regardless of the position of the potentiometer. I've confirmed that the PWM signal is changing correctly, and the hall signals look clean. Would like to confirm this is the correct wiring and board configuration for this motor and figure out why the speed control is not working.
Thank you,
Andy