This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8332: DRV8332 IC not working

Part Number: DRV8332

Hi Sir,

I'm Using DRV8332 IC 

I'Ve given supply voltage is VDD = +12V, GVDD = +12V, PVDD = +24V, 

Out put is 10V PWM when i check the readings with out connecting the motor,

when i connect the motor, it didn't respond.

Motor Part number is 539489.

 thank you.