Hello,
I have several questions on test points in DRV8353RS-EVM (SLV742A) and would like to ask for your advice.
- Is the purpose of Test Points TP1 and TP6 to measure the waveform of Q1? Are TP2 and TP7 to measure the waveform of Q2? If yes, why there were no test points on VM to measure the waveform of Q4/Q5/Q6?
- Could the waveform of Q1 directly measured by probing the connector J6 Pin 3 (MOTC) and lower end of R14? If yes, could TP1 and TP6 be eliminated to save the board space?
- TP6, TP7, TP8, and others are not listed in the BOM. Could they be assumed the same as TP1, TP2, etc.
- The BOM shows TP1, TP2, etc are through-hole test points, which take 4~5 mm in diameter space each in the board. Could they be replaced by SMD test points, which is about 1 mm in diameter? If yes, could the voltage/current waveform of Q1/Q2/Q3 be probed using these SMD test points?
- Majority of test points were placed next to power stage MOSFETs. I am wondering whether it is necessary to place test points on SOA/SOB/SOC pins, INHA/INLA/INHB/INLB/INHC/INLC pins, SPI pins, and/or nFault pin.
- Any advice/suggestions on where to place test points to facilitate the testing of the functionality of the motor drivers board would be greatly appreciated as they are not addressed in the SLVA959A, “Best Practices for Board Layout of Motor Drivers."
Thanks,
John