Hi TI Team,
We are planning to use two DRV8835 Motor driver for Auto focus Lens. VCC and VM is given as 3.3V. My Processor does not have 8 GPIO with 3V3 IO Level to drive both the motor driver, so i have used 2 GPIO with 3V3 IO level and 2 GPIO with 1V8 IO level(Second motor driver is having 4 1V8 IO Level based GPIO). Since Motor driver VIH is 1.65 with respect to 3.3V VCC Supply, it should work.
Could you please confirm the same? If motor driver is having two different IO level, Is that fine?