Other Parts Discussed in Thread: ISO7742, ISO7741
Hi Team,
Can you please advise with request:
"
1- We are using 2 pieces of DRV8860PWP on the same card. We took the control ends of the DVR8860s directly to the processor by making them parallel instead of daisy chain. In other words, DIN-DOUT-CLK-LATCH inserts were used jointly for both. We will check the Fault and Enable ends separately. We planned that the DRV8860 we wanted to drive would be active with ENABLE and the other DRV8860 would passive with its ENABLE tip and communicate in that way. Is such a study appropriate?
2- Do the outputs of the DRV8860, which is disabled in the way I mentioned above, keep their status? For example, what happens if the DRV8860, which is currently driving a solenoid, is passive?
3- There is an information that the DOUT tip DRV8860 is internally pulled up to 5.7V in one of the tables in the datasheet. When you look at the diagram I sent, we isolated the processor side with a DRV8860 using ISO7741 and ISO7742. We fed the DRV8860 side of ISO7741 and ISO7742 with 5V. As you can see in the diagram, we tried to stabilize the DOUT voltage to 5V with the zener acting like a TVS. What is your comment and suggestion about the suitability of this structure?
4- nFAULT ends are defined as open drain. We pulled the nFAULT ends to 5V, which is the voltage level of ISO7741 and ISO7742 as pull up. I don't think it will be a problem, but can you comment if it is appropriate?
"
Thanks in advance
Best Regards
Furkan Sefiloglu