Hi BU:
My customer is implementing the DRV8718-Q1 to drive 4x BDC motor in the project of power seats , now they would like to configure the 8x half bridge output to the
4x H-bridge for the 4x BDC, and the 4x BDC need to be forwards and reverse spin seperatedly.
They won't use the PWM input (IN1~IN4) for the speed adjustment, only set the high side or low side of the half-bridge to spin the motor .
Could you please offer me the register setting for the above requirement , thanks!