This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8702-Q1: VREF pin voltage limit

Part Number: DRV8702-Q1

Hi,

I'm using the DRV8702-Q1 for independent PWM driving. In such conditions I don't need current regulation, so the datasheet suggest connecting VREF directly to AVDD.

My doubt is that AVDD=5V and the recommended operating condition of VREF goes up to 3.6 V. Therefore, should I use a resistor divider to obtain 3.6 V, or do as stated and connect to AVDD? If it is the latter, would the performance/reliability of the part be compromised?

Thanks,

Federico