Hello,
I'm working with DRV8350S-EVM in Sensored mode for my motor application. The evaluation board was working fine with my setup and I was able to test my motor application.
But I have encountered a problem, the GUI is not identify the code dumped in the microcontroller as sensored code. It shows that a new USB connection has been established but the the code is not identified and hence I:+'m unable to run my motor. I found that the D3 LED or FW_Led was not on, which means the firmware was not running in the microcontroller. How can I resolve this issue?
Regards,
Abhishek K Singh