Hello E2E,
When circuit architected at fig.4(from datasheet) that which the direction of rotation of the motor CW or CCW?
Is the standard input PWM frequency to the DRV10866 25-kHz?
Best regards,
ACGUY
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello E2E,
When circuit architected at fig.4(from datasheet) that which the direction of rotation of the motor CW or CCW?
Is the standard input PWM frequency to the DRV10866 25-kHz?
Best regards,
ACGUY
Hi ACGUY,
Thanks for posting your question in MD forum. This device does not have a dedicated pin for direction control. So the direction depends on the sequence of motor phase terminal connections to the device. Range of PWM input frequency is between 15 kHz and 50 kHz.
Regards,
Vishnu