I bought a DRV8256PEVM to test the driver before select it for my new board.
First some incongruences:
- on the product page I read "Up to 1-A peak current", in the manual I read "The components can support peak output currents up to a maximum 4A" while on the silkscreen I read "Board rated for 2.5-A peak for half-bridge". Which is the correct one?
- in the schematic the P version (PWM) requires an high level for the INTERFACE signal, hence R6 should be populated (pull-up). Instead on my board R5 is mounted instead. Why?
- in the schematic there are two voltage settings: 24V or 36V (and set 36V via R2), while on the silkscreen, in the manual and in the product page the maximum voltage is 48V. Again, which is the correct one?
Now I describe the issues using the board. By the way, I need to re-install the software every time I launch it (I'm using Windows 10). When the installation finishes I click "open" and it runs the software. If I close it, I cannot open it again, even restarting the computer. It closes the process in a while without any output (even from console). I need to re-install and open from the installer.
First issue: the right pane shows AIFS 0.5A no matter the position of the current slider. I guess this should reflect the current Itrip settings. What does AIFS actually mean?
Second issue: moving the current slider does not change the Vref on the board. While the other settings lead to a change in voltage (i.e. 0V, 3.3V, etc...) there is no DAC output. Better, both are stick a 970 mV.
Third issue: I removed R27 and R28 to provide an external Vref. Even with both Vref at 3.3V I get a fault condition when the average current consumption is above 1 A.
Fourth issue: the chip becomes VERY hot even at small currents, like 600 mA.
I'm using a DC brushed motor @ 24V. Powering the motor with a constant DC voltage it draws 350 mA. I'm not able to run it with this evaluation board. I tried all settings but I get a fault condition before the motor moves a bit. Only with a fast decay and 32 μs Toff it can barely spin. The current consumption (on my power supply) rises above 1 A at very low speed (IN1 ~ 15%) and I suddenly get a fault condition, with Vref = 3.3V!
Please, would you help me to understand if I'm missing something? The driver should be capable to control motors up to 5A but right now it seems I wasted time and money...