I need to drive solenoid (10 ohm coil) which needs 2.2A for 100mS and after that 0.6A to hold.
Or 24V for 100mS and drop to 12V to hold.
Is it possible to use DRV110? If not do you have any other part?
Thank you,
Goran
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I need to drive solenoid (10 ohm coil) which needs 2.2A for 100mS and after that 0.6A to hold.
Or 24V for 100mS and drop to 12V to hold.
Is it possible to use DRV110? If not do you have any other part?
Thank you,
Goran
Hi,
Thank you for your interest in DRV110. Yes DRV110 can handle 2.2A/0.6A with 24V. Please chose external FET to drive your current load. Then DRV110 control step current level such as 2.2A/0.6A.
regards
Shinya