This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV10983EVM: DRV10983 with QBL4208-41-04-006‎ Trinamic Motor

Part Number: DRV10983EVM

Hi,

I am trying to drive QBL4208-41-04-006 24V‎ 3 phase BLDC motor with DRV10983EVM I purchased recently. So, far I am not having any luck.

I have installed the GUI required and not very sure about the parameters and fault codes.

Any help to debug is appreciated.

Regards,

Sundar.S

  • Hi Sundaresan,

    Thanks for posting on the MD forum.

    First I want to make sure the device is getting powered up properly, what is the voltage on Vcc? Also please ensure that the device is not in sleep mode.

    After you check those two things, I can help you debug further. 

    Any additional information you can provide would be helpful.

    Thanks,

    Michael