Other Parts Discussed in Thread: DRV8873
I'm currently trying to test out and evaluate this device. I've contacted support but apparently need to create a forum thread in order to verify if it's defective. Upon power up and verifying all the connections, the device appeared to work for a second and then stopped due to a fault condition. Since then however, I have been unable to get the device working as intended. I'm using the included software and USB cable to control the device. When taking the device out of sleep mode, a fault is immediately triggered. I remove open load detection and disable ITRIP, but still get a fault when taking it out of sleep. This happens in both PH/EN and Independent Half-bridge mode. In sleep mode, when changing over to PWM mode, a fault condition is immediately triggered and this is before I sleep mode is even disabled. The fault condition is noticed via the red LED on the board and through software. As I have the hardware version, I'm unable to determine what the actual fault is as it does not report specific fault data. Any help would be appreciated to verify defectiveness. My VM voltage is 18V and I confirmed that the motor is the correct type for this device and is fully functional. thank you in advance.