Other Parts Discussed in Thread: DRV8353R, DRV8353
Hello Team,
I am using “DRV8353R – 100-V Three-Phase Smart Gate Driver” there are below queries I have could you help me for the same
- Setting Current Threshold: By using VDS overcurrent protection (OCP): VDS overcurrent trip voltage "DRV835x: VDS_LVL" by using OCP Control Register (address = 0x05h) OR VSEN_OCP: VSENSE overcurrent trip voltage "SEN_LVL" CSA Control Register (DRV8353 and DRV8353R Only)
- Other than Fault(29) pin is there any INTP present? If yes what are the Interrupts OR if No : How can I disabled Fault pin ? -> in GDU enable mode)
- Charge Pump (VCP) how to make enabled & Disabled : CPH(4) & CPL(3)
- Setting up Driver output high : is the process followed is correct? INHA(34) > high, INLA(35) > Low accordingly GHA(8)>high GLA(9)>Low & what about SHA(9) pin status?
- Does SHA(9) pin is used as feedback for Driver output status
- Reading of “Charge Pump Voltage”: "How can we get the voltage is there any specific resistor"
- How can we read GDU state, (Sleep/Enable/Fault)?
- How can we get/read present current value? (that is used for checking with actual over current setting)
- How can we get/read present voltage value? (that is used for checking with actual over voltage or under voltage setting)