Hello to everyone, I bought some drv8825 chips in order to build a 3D printer, after I designed the carrier boards, I installed four of the chips, then when I tried to test the drivers I came across a very unusual problem, three of the drivers when in use they didn't keep the same direction, I measured the voltage at the direction pin and during test there was a constant voltage of 4.97 volts, I measured the voltage at the trimming pot and there was a constant 0.4 volts, i cannot explain myself why is this behavior, I also changed the stepper motors (the stepper motors are recovered from diferrent printers) but the problem persists. What is strange is that the fourth board works perfect, it doesn't have these symptoms.
Could please someone help me !
This is how the boards look like