Hello,
Recently produced a prototype that uses the DRV8312 to drive a sensored BLDC motor. I'm having an issue where any time I try to drive any of the motor phases, both the OTW and FAULT lines fire off immediately and disable the device. I have checked for any shorts to ground and can not locate any. The OTW fault is especially peculiar, as the device is just at room temperature. Does anyone have any ideas? Is my chip dead? This is the second one I have installed with the same issue. I've read the datasheet through several times and I can't find any issues with my schematic that would cause this behavior. These faults occur even with the load disconnected. There is 12V present on all power pins, and 3.3V at VREG. The motor does not spin at all, only a faint click before the FAULTs trip.