Part Number: DRV10983Q1EVM
Hello Sir/Madam,
I am trying to spin a 6V BLDC with the DRV10983Q1-EVM by connecting the three phases to U,V,W and supplying 7V. I have programmed phase resistance and Kt value by:
1. Measuring no load resistance between two phases and dividing it by 2
2. Kt= [6/(40,000 rpm/60/2 pole pairs)] ~ 18 mV/Hz . I have tweaked the value of Kt by +- 30% from this value to get it up and spinning.
However, I see a back EMF error Code 2 as the system moves to closed loop. This however does not stop motor operation as I have disabled lock detect on the software GUI. I would like to understand what am I doing wrong and if this would affect the torque curves and characterization of the motor?
Please see attached image above.
Thanks,
Ganesan M.