This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BOOSTXL-DRV8301: Motor Specs for the LVBLDC-LB-BNDL (Motor Part - DN4240S24-026-TI)

Part Number: BOOSTXL-DRV8301
Other Parts Discussed in Thread: MOTORWARE

The Motor Drive Bundle LVBLDC-LB-BNDL sold by TI contains a motor of which no specifications are included or mentioned. In order to use the MotorWare lab manual these specs need to be set. If someone from TI or the supplying company (Telco Intercon) could provide them it would be very much appreciated. I should note that there is some information for a motor posted here but careful inspection of the part number reveals the part in the kit is a DN4240 while the specks on the page are for the DN4241. 

Thankfully 

Kas