This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

DRV8839EVM: Question of the DRV8839DSGR's Operation Voltage Range

Genius 14850 points

Replies: 1

Views: 415

Part Number: DRV8839EVM

Hi Sirs,

Would you please advise that if we can use 5V VM and 1.8V VCC, while the test conditions on the datasheet is 3.3V VCC?



Thank you and Best regards,

Wayne Chen
12/22/2017

  • Hi Wayne,

    Yes, the DRV8839 can use VM=5V and VCC=1.8V.

    Best Regards,
    Rick Duncan
    Motor Applications Team

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.