Other Parts Discussed in Thread: DRV11873, , DRV11873EVM
Hi
Does DRV10983 have current limit function those like DRV11873 has?
The current limit of DRV11873 can limit the current to motor.
It would be helpful because motor speed can be controlled just by PWM without increasing current flows.
Our motor can spin with DRV11873EVM up to 9000rpm.
However, it could not spin up to 9000rpm with DRV10983 because of overcurrent protection (triggered at 3.2A).
Do you think it is possible to spin our motor using DRV10983 up to 9000rpm depending on motor tuning?
BestRegards