This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV10866: Yes

Part Number: DRV10866

It can not to drive the motor to work,Please help to check it.Thanks a lot

First picture is the Schematic diagram,the second is PCB,the last picture is the waveforms of one phase.

  • Wei,

    Your schematic and layout appear to be fine.

    Is channel 1 the PWM input signal? If so it needs to switch from 0 to 2.3+ V. It looks like it switching from ~3.3 to 4.8V. Also, the frequency of the PWM input needs to be between 15 and 50 kHz. I'm seeing 227 Hz.

    Can you show scope with Phase U current, PWM input and FG output?

    Thanks,

    Brian