Part Number: DRV10983
Hello,
I am working on ceiling fan with Brushless DC motor, and
My EEPROM configuration registers are:
- (0x20)MotorParam_1 == 0x4D
- (0x21)MotorParam_2 == 0XE9
- (0x22)MotorParam_3 == 0x4A
- (0x23)SysOpt_1 == 0x64
- (0x24)SysOpt_2 == 0xDB
- (0x25)SysOpt_3 == 0xFD
- (0x26)SysOpt_4 == 0x77
- (0x27)SysOpt_5 == 0xBC
- (0x28)SysOpt_6 == 0x7B
- (0x29)SysOpt_7 == 0XF9
- (0x2A)SysOpt_8 == 0x79
- (0x2B)SysOpt_9 == 0x0E
FaultCode Register gives 0x00 or no error.
What happen is:
1- When I start power supply at 24V DC current pointer in the power supply swing between 0 to 0.4A and fan doesn't spin.
2- I decrease voltage of supply from 24V DC to 15V DC, current drawn by driver increase and fan spin at slow speed then I increase voltage again to 20V DC current drop to zero and fan stop spinning.
So, please can you advise me which me which parameter could effect on previous behavior and make fan spin properly?
Is something in parameters above?
--
B.R.