Hi, I'm some help with DRV8305-Q1EVM.
I compiled proj_lab02b and ran it with InstaSPIN Universal and a BLDC motor, 60KV, 7 pole pairs after selecting the 'test motor' in user.h and changing USER_MOTOR_NUM_POLE_PAIRS to 7, it trips half way through the ramp up phase, then shudders at the end of the test and lights the red led labled nFault on the EVM board, though it does say it has identified, however because the fault led is lit it wont respond until cleared, where it loses its ID. What should I change to successfully identify this motor without tripping into a fault state?
Thanks,
Neil