Part Number: DRV8432
Hello,
Following to the customers wish we have implemented an external bootstrap voltage option according to the TI proposal, please see the attached document. The external bootstrap voltage is isolated and related to the 48V supply.
We have noticed that when the High-Side-mosfet is ON, the output voltage of the bridge is 33V, while the bootstrap voltage is only 42V.
So we reduced 24K resistor to 2K2, we obtained 47,4V from the bridge output, and bootstrap voltage changed to 56V. So far so good.
Due to the reduced resistor value we have increased power loss when the High-Side-mosfet is OFF and the output is Low. It’s appr. 1W, because the bootstrap voltage is 13V and external 12V_ISO is 60V (seen from GND). Please find the attached schematic, the mosfet's switches below are for external bootstrap volltage while the driver is in the reset state.
Is that a wrong way to reduce the 24K resistor to 2K2? In this case we have got 1.8mA current flowing into the “BST_A” pin. What is the reason for such a high value of 24K?
Best Regards
Vitali