Part Number: DRV10983EVM
Other Parts Discussed in Thread: DRV10983
How can i get the motor running? It moves very short and stops. After a few seconds the motor restarts.
To enter value of windig resistance, i found no way of entering 0.31Ohm. Displayed value jumps to 0Ohm.
I tried to follow application note AN_DRV10983 but with no useable result.
The motor has 0.31Ohm resistance, runs at 24V with maximum power 50W. (300..5000rpm)
Stator has 6 coils.
For my purpose, lower speed operation at 20W seems to be sufficient.