Part Number: DRV8432
I have the same question. Since we cannot presently get DRV8432, can we use DRV8402 in it's place for the time being? I see that the absolute voltage range is 65V rather than 70V - what other big differences are there?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DRV8432
I have the same question. Since we cannot presently get DRV8432, can we use DRV8402 in it's place for the time being? I see that the absolute voltage range is 65V rather than 70V - what other big differences are there?
On paper, the absolute voltage rating and current rating of the DRV8402 is not as high as the DRV8432. Also, there is a slight difference in the current limit threshold using the same resistor value. Finally, there are a couple of HB modes in the DRV8402 that are not used (reserved) in the DRV8432. Whether there are other differences I don't know, plus we haven't tested it yet.