This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8834: Indexer mode configuration

Part Number: DRV8834

Hello,

Our customer use the DRV8834.

The voltage of the VM is 5V.

To reduce the signal line, they connect the nSLEEP to VM directly.

They want to use the DRV8834 with Indexer mode, so the CONFIG set high.

They have a question about CONFIG pin.

It is mentioned "State is latched at power up and SLEEP exit" on the datasheet.

Is it possible to connect the CONFIG pin to VINT pin directly?

There may be delay time from SLEEP exit to VINT is high....

Best Regards,

Naoki Aoyama