Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BOOSTXL-DRV8305EVM: Current scaling

Part Number: BOOSTXL-DRV8305EVM
Other Parts Discussed in Thread: DRV8305, DRV8323

I am using LauncpadXL 28379D + DRV8305EVM.

DRV8305, Gain is 10 V/V, Rshunt resistance is 0.007 ohm (DRV8305EVM) .

max input current, +19.3 A = 3 V from DRV 8305

Input current, 0A = 1.65 V from DRV 8305

What is the max negative current read by DRV8305?

What is the voltage output of DRV 8305 at its max negative current? 

I need this information for calibrating the current. I am little confused over here. I want to clarify myself. Thanks.