Other Parts Discussed in Thread: , LM2596, DRV10974
Are the flyback diodes neccassary or not while using DRV11873 or/and DRV11873EVM ?
I am using max 16 V. 300 mA.
Thank you.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Cole Macias,
I never could think these diodes could serve the same.
Thank you very much for your time and interest.
King Regards,
Oguz Coskun
Hello Mr. Cole Macias,
I am a beginner / amateur on electronics and motor control / design.
I have build the motor of my own design, cooling fan.
This propeller's 17 magnets have all the same polarity. (not NSNS but NNNNN or SSSSS)
9 x 3 = 27 coils are all in the same direction too.
Normally this motor is designed to work with Hall Effect sensors and a TTL circuitry. And it works very well with 16 V. 300mA.
When I tried to control it with DRV11873EVM with solar energy, it works very well too. 19,5 V solar panel: (4 x 1.5 V 100 mA) + (9 X 1.5V 250mA) and a LM2596 regulator .www.ti.com/.../lm2596.pdf
I am trying to build more of this hande made / recycled papers motors. I want to make it more efficient and lower cost.
I have already bought DRV11873 chips and necessary elements to soldier DRV11873 motor control circuits.
Do you have any suggestion about this motor and motor control circuit ?
Thank you very much for your time and interest,
King Regards,
Oguz Coskun
ouzcoskun.com
design2011.net
Hello,
Now I have 18 coils and 12 x 3mm. magnets. It is working very well with DRV11873 EVM. (12V. 260 - 300 mA.)
How about this PCB design ?
I have used the same circuit on the DRV11873EVM board but some parts have different SMD packages.
Thank you very much for your interest and time.
King Regards.
Hello again Oguz Coskun,
I think the layout guidelines in the datasheet does a pretty good job with what I would recommend.
A few further comments:
For example, I assume C1 and C3 are decoupling capacitors for VCC. I understand that the phase and com traces are blocking the path but I'm confident that some shifting could allow you to move the decoupling capacitors closer. If the device demands more charge from VCC, right now, the charge has to go through 2 vias (which is stray, series inductance) and a longer trace (which is more resistance) until the charge can be delivered to the device. And the GND potential all has to go from the GND pin, through some more vias, then to the other side of the capacitor. You can think of this as an LC circuit where high frequencies (e.g. fast demands for current) will resonate and cause spikes that can disrupt the rest of the circuit. While it may work in this design, good layout technique prevents something like this from happening. You should consider this for the other important capacitors as well.
Also, I do not see a ground pour (or the bottom layer). Right now it looks like the power pad is floating (because there are not vias and it is not connected to pin 8, GND). The power pad dissipates heat and allows charge to spread out so it does not create a potential difference between two points on a GND plane. Consider putting a large pour on the top and bottom with many vias stitching the grounds together between the two layers.
A comprehensive layout guide can be found in this app note: http://www.ti.com/lit/an/slva959/slva959.pdf
Best,
-Cole