Part Number: DRV8840
Other Parts Discussed in Thread: LMD18200,
Hello
I have almost the same problem with the theme https://e2e.ti.com/support/motor-drivers/f/38/p/654636/2416686?tisearch=e2e-sitesearch&keymatch=DRV8840%20noise#2416686
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DRV8840
Other Parts Discussed in Thread: LMD18200,
Hello
I have almost the same problem with the theme https://e2e.ti.com/support/motor-drivers/f/38/p/654636/2416686?tisearch=e2e-sitesearch&keymatch=DRV8840%20noise#2416686
My motor is maxon re35: 24V, 0.2mH, 0.6 ohm.
The pcb board is designed almost the same with the datasheet. The nRESET is connected to the mcu with 3.3V voltage. PWM frequency is 30~48kHz.
The motor has "ZZZZ..." noise and the out- and out+ is not stable whatever the duty is (0%~50% all tried).
What can I do?
Thanks!
Hi Rick!
Thanks for reply!
The input and output signal are shown in the first figure.
In the second figure, the output PWM frequency blinks from 31kHz to 48kHz and the most time about 31kHz. The motor still has "ZZZZ" noise.
With the same condition, I have tried LMD18200T. The motor has no any noise .
So why and what should I do?
Thanks!
Ziv
hi Rick:
I have tried different PWM duty with input width larger than 1us, typically larger than 10us. The output looks normal but the motor still has "ZZZ" noise.
With the same test condition, LMD18200 has no noise.
The size of DRV8840/8842 IC is small and a good option for my application. But the noise is undesired.
What can I do further?
Thanks.
Ziv