Dear Sirs/Madams-
I have worked with the DRV8301 extensively via the DRV8301 individually and the DRV830x-HC-C2-KIT_v105 kit and the DRV8312-C2-KIT_v128 kit and the HVMotorCtrl+PfcKit_v2.1 kit. I am now to the point where I have to increase the amount of current and power significantly. I am estimating that I will have to place 6 NMOS MOSFET's in parallel for one leg of a 6 way/3 phase bridge. The combined gate capacitance of one leg (6 MOSFET's) is about 25 nanofarads. Document SLOS719F.pdf, Page 26, Equation 3, Section 8.2.2.1 "Gate Drive Average Current Load" is 30mA and indicates the possible limits of the DRV8301 trying to drive 36 MOSFETs (and also page 15, third paragraph, limits to 30mA). I have found another TI document that requires study (SLUA618A.pdf, specifically starting on page 6) on my fundamental short comings of understanding this issue.
In the meanwhile, can you recommend some TI high side/low side driver gate driver products that may be suitable for my application?
Thanks,
Kurt