Other Parts Discussed in Thread: DRV8701
Hi team,
According to the datasheet, DRV8873 has a 10A-peak current drive but there is no current specification in abs,max rating and recommended operating conditions.
(1) Is there really no current specification of abs.max rating?
Considering the Ron from the characteristics, DRV8873 would be >2W power in case of 5A continuous operation at 50degC.
(2) Do you think we can use DRV8873 in 5A continuous operation at 50degC in spite of reaching at >2W power?
Regards,
Jun