Other Parts Discussed in Thread: DRV8353, MOTORWARE, CSD19532Q5B, LMG5200, , TMS320F28027F
Hello,
I am designing a custom board by trying to use the DRV8305 and the F28069 combo, but the DRV8305 has a voltage limit of 60V. My supply voltage will be around 65-70V, so I was thinking of using the DRV8353, but I could not find the files for using DRV8353 in Motorware along with F28069. So I want to know if I can use DRV8305 along with CSD19532Q5B MOSFETs for an ACIM control using InstaSPIN, BUT giving only 5V supply to DRV8305 and 70V supply to the FETs? Is 5V too low for the DRV8305 to operate? I am sorry if I violated the forum rules, just had this doubt that I needed some clarification on. If anyone can answer this, that would be great.
Thank you,
Ally