Dear all,
Could you give me some advice about the following content.
Our customer measured motor current and both-end voltage of R2 in following circuit diagram.
※Our customer's situation
VM=6.0V
VIN1,VIN2=3.3V
C4:ceramic capacitor
As the results of measurement, the following waveform data is measured.
As shown in the above waveform, when the motor is driven, the motor current is suppressed to about 1A by the function of the current detection resistor.
However, a 1.5 V peak pulse was observed at the both-end voltage of R2 just before the transition to the slow decay mode.
Although it is equivalent to about 7.5A in current conversion, such fluctuation is not seen in the motor current waveform.
We believe that DRV8833's dead time caused this peak.
When we confirmed the waveform data, the width of this peak seems to be about 500 ns.
According to datasheet, tDEAD(DEAD TIME) is 450ns(typ,VM=5V) and this value is close value compared the value from waveform data.
Our customer would like to know the cause and solution of this phenomenon .
It would be great if you could let me know your thoughts this cause.
Y.Ottey