This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

DRV8303: voltage drop at GVDD after EN high

Expert 3510 points

Replies: 5

Views: 219

Part Number: DRV8303

HI,

my customer is facing some issues with the DRV8303.

 

~ 20ms after switching EN_Gate to high the DRV8303 shows a voltage drop at GVDD (green voltage in the attached scopeplots).

This happen before a MOSFET is switched on (see second scopeplot). At low battery voltage of ~15V the GVDD voltage can drop down below 7V.

 

What is the issue for that ?

The DRV8303 showed from time to time an undervoltage flag in the failure memory for GVDD.

 

Capacity between GVDD and GND ~ 10uF MLCC

Best wishes,

Olrik

  • Olrik,

    I didn't see the image as mentioned, please reupload it.

    Regards,

    -Adam
  • In reply to Adam Sidelsky:

    Hi Adam,

    pls see attached the missing plots.

    Best wishes,

    Olrik

  • In reply to Olrik Maier:

    Olrik,

    Checking the phase current ("phasenstrom") will not correlate with the gate signals turning on. Can you repeat the plot above but showing the High side and Lows side gate of one phase?

    Regards,

    -Adam
  • In reply to Adam Sidelsky:

    HI Adam,

    I have done some additional measurements and yes, we have here two short switch on pulses on GL_C, followed by two switch on pulses on GH_C. These pulses are not during the same time. Also no other MOSFET is switched on in this period of time. The first pulse should be as long as the 2nd one but I think due to the drop in GVDD the gate will be switched off again.

     

    Nevertheless we can see this drop of GVDD here. During normal operation this drop cannot be observed. A delay of additional 10 ms between start up and switching this pattern also do not help.

    Measurements by email

    Best wishes,

    Olrik

  • In reply to Olrik Maier:

    Olrik,

    Since this is being handled by email and the issue is on hold, I am closing this thread as it cannot stay open and inactive.

    Regards,

    -Adam

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.